Hi
If two Redrivers (TUSB1002ARGER) are strung together, what are the lengths they can support at the front and back?
CPU----1----->TUSB1002A---2--->TUSB1002A---3--->USB connector
1 and 2 and 3 lengths they can support?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
If two Redrivers (TUSB1002ARGER) are strung together, what are the lengths they can support at the front and back?
CPU----1----->TUSB1002A---2--->TUSB1002A---3--->USB connector
1 and 2 and 3 lengths they can support?
Hi,
Each 1002A can support a max of 15.3dB of loss on the RX channels.
This means each length (1, 2, 3) should have a loss no greater than 15.3dB. You need to find the loss/inch of your PCB trace to get an accurate length estimate.
A few things to keep in mind:
1. Your CPU needs to compensate for the loss coming from the first 1002A. If your CPU cannot compensate 15.3dB then length 1 will need to be shorter.
2. The USB cable attached to the connector will add loss to the signal path. I recommend keeping length 3 shorter than 15.3dB to account for this loss.
Best,
Shane