Part Number: ONET1101L
Hello,
I want to use the ONET1101L chip to drive the laser diode. In the process of looking at the datasheet, I saw that the input terminal DIN+ and DIN- are forward input terminal and reverse input terminal respectively.
I want to know:
1. Is this input signal a pair of differential signals?Can the single-end signal be triggered?If yes, how should I connect the two pins?
2. What is the effect of the level of DIN+ and DIN- on the chip pin MOD+ and MOD-, and what is the effect on the driving laser light?
If possible, please provide a design specification.