Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75174: LTC 487 CSW #TRPBF alternative

Part Number: SN75174
Other Parts Discussed in Thread: DS34C87T, AM26LV31, AM26C31, DS34LV87T

Hi team,

Could you help recommend the alternatives of LTC 487 CSW #TRPBF? 

P2P is better, and I found SN75174 could meet the need, but it seems old, do we have newer recommendation?

Thanks

Lillian

  • DS34C87T/DS34LV87T are P2P. Nowadays, the AM26C31/AM26LV31(E) are much more common.

  • Hi Lillian,

    The SN75174 is technically the correct match because the comp. device supports RS-485 and RS-422. 

    If they don't need RS-485 and only need RS-422 compliance then the AM26C31 has been recently redesigned and is "similar" in operation and the same pinout. 

    The devices Clemens mentioned also could work - but they are also only RS-422 and not RS-485 + RS-422. 

    Best,

    Parker Dodson