Part Number: DS250DF230
Hi,
1) “7.15 HEO/VEO Lock Monitoring” in the Programmer's Guide (SNLU182G) states:
"Enable or disable Horizontal Eye Opening (HEO) and Vertical Eye Opening (VEO) monitoring for CDR lock qualification. HEO/VEO lock monitoring will cause the CDR to fall out of lock if the HEO or VEO fall below the configured threshold."
By “below the configured threshold ” do you mean “the threshold or less”?
Or do you mean “less than the threshold ”?
2) I think It will lock when the threshold set by 0x6A is exceeded.
Do you mean “more than the threshold ”?
Or do you mean “the threshold or more”?
Best Regards,
Nishie