Part Number: TUSB320
I'm hoping to use TUSB320 in GPIO mode on a device permanently configured as UFP. To comply with the USB standard (USB Type-C Cable and Connector Specification 2.3 (Oct 2023) section 4.6.2.1) my device will have 60ms to adapt its current sink maximum after the source advertises a change in its capability. I know that TUSB320 only measures and reports the initially advertised current on the GPIOs. However, can I force TUSB320 to update its measurement by toggling the EN_N pin at intervals? My reading of the datasheet suggests that the answer is "yes" because of section 8.3 (here I assume that this sequence of events occurs whenever the EN_N pin goes from high to low in addition to whenever Vdd ramps up with EN_N held low). I'd like to confirm my understanding. Thanks!