Part Number: DS90UB948-Q1
Other Parts Discussed in Thread: TAS2505, , DS90UB925Q-Q1
Dear Specialists,
My customer is considering SER (DS90UB925) and Des (DS90UB948) and has a question.
I would be grateful if you could advise.?
---
I2S data from the I2S master to audio amp(TAS2505) via SER (DS90UB925) and Des (DS90UB948).
Data bits are 16 bits.
When the bit clock is lowered, 2kHz audio cannot be played.
situation
(1) To play a 2kHz pure tone with TAS2505,
When I sent sine wave data from the I2S master to TAS2505 at LR CLOCK8kHz, I could not play the sound.
(2) When I raised the BIT CLK and set the LR CLOCK to 32kHz, I was able to get the desired sound up to 1kHz, but the sound was different above that.
(3) By further increasing BIT CLK and setting LR CLOCK to 64kHz, it is now possible to play up to 2kHz.
question
(1) The sound cannot be played unless it is transmitted with an LR CLOCK that is at least 32 times the frequency you want to play.
Is there a setting error in SER(DS90UB925) Des(DS90UB948)?
(2) Regarding DS90UB948, the Des register “7.7.1.49 I2S_DIVSEL Register (Address =0x3A)”,
When used with the reset value (0x0), will the clock input to serializer be output from Des as is?
Please let me know how it is converted.
(3) Is there a relationship that should be observed between I2S bit CLK, I2S CLK, PCLK (Serializer) and MCLK (De-serializer)?
---
I appreciate your great help in advance.
Best regards,
Shinichi