Part Number: MAX3243
Hi Team
do we have MAX3243 reference design SCH for DSUB9?
BRs
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
I don't believe we have a reference schematic for that but we have an FAQ that includes a 3T5R RS232 device connected to a RJ9 (Dsub9) connector.
Figure 8 in this document would be how you could make a connection like that.
-Bobby
Hi Bobby
Thanks for your reply :)
could you help on this SCH review?
BRs
Brian
| U1: MAX3243 | ||
| Checked | Status (Good, Bad, Okay, ?) | Additional Comments |
| Schematic pinout matches datasheet pinout | Good | |
| Net names matches expected pinouts | Good | |
| Local decoupling caps | ? | I see some additional 0.1uF caps by J1, please make sure they are placed close to Vcc of MAX3243A |
| Input pins aren't floating | Good | Customer setup has auto-powerdown enabled (No issue, just stating this) |
| Charge caps match datasheet suggested values | Good | |
| SUB9 net names match expected pins | Good | I checked this based on the document I referred you to in my earlier post |