This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65LVDS31: SN65LVDS31/33

Part Number: SN65LVDS31

Hello,

Below is a diagram of the system. From the differential source to the line driver (SN65LVDS31/33), I have a 15 feet cable and 3 feet to the SPI Master. Do you think I will have issues with the clock and timing if the master SPI clock is 7 MHz?

Regards,
George K.