Part Number: TUSB8041A
hello. everyone,
I am trying to connect two infineon's CX3 (mipi to usb3.0 Controller) with TUSB8041A.
The maximum output of CX3 is 2.4Gbps. The maximum input my PC can receive is 2.4Gbps? Or is it 4.8Gbps?
thank you,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TUSB8041A
hello. everyone,
I am trying to connect two infineon's CX3 (mipi to usb3.0 Controller) with TUSB8041A.
The maximum output of CX3 is 2.4Gbps. The maximum input my PC can receive is 2.4Gbps? Or is it 4.8Gbps?
thank you,
USB 3.0 data rate is 5Gbps , If CX3 is mipi to USB 3.0 bridge, then CX3 should convert mipi 2.4Gbps to USB3 5Gbps.
Any PC which can support USB3.0, it should support 5Gbps.
TUSB8041A can support 5Gbps as well
Regards
Brian