Hi Team,
My customer is using SN65LVDS3487 IC in their design. They are seeing attenuation of the output differential signals from SN65LVDS3487 while connecting the receiver electronics ( Load ). In no load condition the output differential signals swing is +/- 3.3 V for a LVCMOS compatible (3.3 V) input signal - can you help confirm if this is okay. Also, please help provide a solution for the above issue.
Thanks,
Jash