Other Parts Discussed in Thread: TCAN3414, TCAN330
Could you please let know the slew rate which is needed for having a maximum data transfer of 1Mbps . This would be helpful to choose the RS pin resistor.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Could you please let know the slew rate which is needed for having a maximum data transfer of 1Mbps . This would be helpful to choose the RS pin resistor.
As a rule of thumb, the rise/fall time should be less than one tenth of the bit time. So assuming VOD = 2 V, the limit would be 2 V / 100 ns = 20 V/µs, i.e., you should not use any resistor at all. (This is plausible because you are using the transceiver's maximum data rate.)
In this case , As per the graph mentioned in the datasheet , for 20V/us , it is almost 0kohm , should we tie the Rs pin to GND in this case?
Is this same for SN65HVD234 as well? In below graph it is mentioned as HVD233?

Thanks Clemens!
Hi Asha,
I agree that for use with the maximum data rate for this device that a 0-ohm resistor should be used for the slope control input.
Please also consider the use of a newer device such as the currently available TCAN330 family or upcoming TCAN3414 family. These devices a offer better cost structure and overall performance compared to the older "SN" part numbers. They are also mostly pin compatible with older transceivers so updating older designs should be possible, and integrating into new designs is easy. Let me know if you have any questions on these devices and how they may benefit your application.
Regards,
Eric Schott