Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] I2C Protection

Back to Interface Home Page

I2C Protection

Highlights:

  • 2 Lines to Protect
  • Low Capacitance required to minimize signal interference
  • Speeds up to 5Mbps

TI Products Recommendations

Working Voltage (V)

IEC 61000-4-2 ESD Rating (kV) (Contact)

Capacitance (pF)

Channel

count

Package Size (mm)

Package

Polarity

TPD1E01B04

3.6

15

0.18

1

0.6 x 0.3

0201

Bidirectional

TPD1E10B06-(Q1)

5.5

30

12

1

1.0 x 0.6

0402

Bidirectional

ESD451

5.5

30

0.5

1

0.6 x 0.3

0201

Bidirectional

TPD2E2U06-(Q1)

5.5

25

1.5

2

1.6 x 1.6, 2.0 x 2.1

SOT-523, SOT-323

Unidirectional

< Related Threads>

Which Polarity Protection Does I2C Require?

Will ESDS302 Protect I2C Systems?

Will TPD2E2U06-Q1 Protect I2C Systems?

Where to Test I2C ESD?

3.3V 400KHz I2C Protection

5.5V I2C Protection

ESD and EFT Requirements