Part Number: DS100MB203
- Does MUX support the loopback feature and how do I configure it?
- What is the insertion loss of MUX?
- Can we know how EQ works by *.sh config files?—— is set by an external PIN or an internal register?
In our schematic, EQ S0/S1 is a pull-down 1k, and EQ D0/D1 is a pull-up 1k,Is it *.sh config files or external pins that determine how MUX works? - According to table2, the Float and R only be configured by pull-up or pull-down resistors,the 0 and 1 only be configured by code,right?
below is schematic\Table2\*.sh config files
DS100MB203_SCH_0417.pdf
ds100mb203_setup.zip