Part Number: DS90LV001
Other Parts Discussed in Thread: SN65LVDS17
Hi,
Is there any LVDS buffer with VCC=2.5V just like DS90LV001 except of VCC=3.3V;
requirements:
VCC=2.5V
LVDS; 600MBPS
LVDS channels; 1 or 2.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DS90LV001
Other Parts Discussed in Thread: SN65LVDS17
Hi,
Is there any LVDS buffer with VCC=2.5V just like DS90LV001 except of VCC=3.3V;
requirements:
VCC=2.5V
LVDS; 600MBPS
LVDS channels; 1 or 2.
Thanks for the help Clemens.
Ken,
An engineer has been assigned to this thread, but please be patient as they are out of office until Monday. However, Clemens suggestion is correct.
Regards,
Eric Hackett
hi, all
SN65LVDS's input just only support PECL and its output can support LVDS, it can't support LVDS input, is it right?
Yes; its inputs are described as "differential" but are PECL.
For how to connect LVDS signals to a PECL input, see figure 9 of DC-Coupling Between Differential LVPECL, LVDS, HSTL, and CM. But note that the voltage dividers are designed to get 2 V from a 3.3 V supply; for 2.5 V, use 62 Ω and 250 Ω.
Hello,
I put the criteria above into the LVDS search tool. Here is the link with the options:
LVDS, M-LVDS & PECL ICs product selection | TI.com
The SN65LVDS's can be configured to accept single-ended PECL signals by using the internal Vref / Vbb. If you wish to configure for LVDS, leave this pin unconnected or open and ensure that the input signal meets all recommended operating conditions, such as for Vic (common mode input voltage). As shown in Clemens's figure, external modifications would be required to achieve these operating conditions if interfacing LVDS <-> LVPECL signals.
Regards, Amy