Part Number: DP83822IF
Hi,
We, at Teledyne, use the DP83822IF in our design. We purchased multiple DP83822 EVM boards. Our design and of course, the demo board work fine in 100BaseT which is what we use. We are now trying to convert our design to support Fiber Optics also.
The Eval board and the manual shows the changes required to change to F/O. To baseline the design, I wanted to make sure the Eval board works in 100Base-FX after making the list of changes. I did the following:
1-converted the Eval board per instructions on sheet 18. I also matched the termination requirements for the SPF transceiver that I am using with PECL logic.
2-Inserted SD-SxAA1-D11 SPF optical transceiver
3-cabled to a "SFP Fiber to Ethernet Media Converter" with the same SD-SxAA1-D11 SPF optical transceiver
4-Power up - I do not see any link indicating that it works.
Q1 - Any idea what could be wrong?
Q2 - Do you offer any eval boards that are already in F/O mode that I just insert a F/O transceiver and see the link to the converter? Just in case the HW MODs to demo board are wrong!
Thanks
Magid