This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DP83822H: How do I configure MDI swing levels to assist with VoD compliance?

Part Number: DP83822H

When testing DP83822 for PMD compliance testing, it may be required to adjust the swing level of the device if the levels are outside the range. A first check would be to ensure the schematic and layout design are the most optimal for testing. If the design is fixed, a way to correct for this would be to utilize Reg 0x403. However, when using this register, it is important to implement a soft restart (Reg 0x1F = 0x4000) immediately after configuring the register to implement the changes made.

Please note that this register requires extended register access.