Part Number: DS90UH948-Q1
Hello:
1. When HDCP content protection reaches the deserializer, the output data from the deserializer to the display is decrypted. How to configure registers to enable UH948 UH949 HDCP function?
2. Can you provide information on the HDCP testing and certification process?
3. The manual introduces HDCP. What registers do customers need to configure to enable HDCP functionality?
4. After the HDCP function is enabled, can it be directly handed over to a third-party (ATC) certification agency for HDCP certification and licensing?
5. Which HDCP license is more suitable for the process of HDCP certification? HDCP v1.4, as shown in the figure below, should be selected between these two versions. Is your understanding correct?