Part Number: TMDSLCDK138
Other Parts Discussed in Thread: TVP5147M1, OMAP-L138
Daer E2E / Support,
I have an OMAP LCDK L138 development board, as you might already know it comes in with various components, some listed below:
1) TVP5147M1 Video Encoder,
2) Winbond W971GG65B
3) FTDI Serial
4) AVC16T245
5) 4 x LEDs
etc
I was looking for a document to show how the pins are connected between the OMAP L138 chip and all other components (some that's listed above), something like:
Omap-L138 PIN-A10 -> Connected to TVP5147M! Pin-4
I am asking as I need to communicate with these chipsets but have no information on which pins to use.
If there is any other "direct way" to connect instead, i.e. such as using a special API for the LCDK to say "display red-screen on VGA" then that would also help.
Right now, I cannot find any documentation on TI (web, forums, support, E2E) to help with how to develop the LCDK further.
Thanks & Regards
Heider