Part Number: DP83867ERGZ-R-EVM
Connected to XILINX ARTIX7 FPGA
Ran external connections @ 1GbE to Wireshark on laptop. Tx good, Rx nogo
Tried loopback, crossing A - B @ 100MbE, directly connected at RJ45. Tx good, Rx nogo
In both situations, Ethernet signals are measured at the PHY chip, the Rxclk is active 2.5MHz, but no signals on RxD0-3?
Are there registers in PHY chip preventing this output back to FPGA? Physically do not measure anything coming out on a scope? This occurs on 2 different boards, and have replaced the PHY on 1 of those, so 3 PHY chips.
Thx!