Part Number: TCA9617A
Other Parts Discussed in Thread: TCA9517-Q1, , LSF0102-Q1
Is there a similar part number that is automotive grade with a higher operating temperature?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TCA9617A
Other Parts Discussed in Thread: TCA9517-Q1, , LSF0102-Q1
Is there a similar part number that is automotive grade with a higher operating temperature?
Hi Kerry,
We offer TCA9517-Q1 which is AEC-Q100 qualified (-40C to 125C)
This device is only validated for standard mode and fast mode speeds (0 to 400kHz). If 1 MHz buffer is needed, TCA9617A/B is our only option at the moment.
Regards,
Tyler