Part Number: TUSB8020B
Please verify the number of USB interfaces supported by the TI chip;
From the diagram, it can support two USB2.0 and one USB3.0 simultaneously;

From the chip pin diagram, it can support 2 USB 3.0;

If it is not possible to support two USB 3.0 chips at the same time, please help recommend a cost-effective chip that can support two USB 3.0 chips at the same time.