Part Number: TLK106
Other Parts Discussed in Thread: DP83822H
I would like to implement a transformerless connection between Phy on a daughter card and a second phy on the main board it sits on. Distance between the two PHYs is less than 10cm.
Figure 10 shows a single cap isolation topology of AN-1519 shows a single cap isolation topology.
AN-1519 DP83848 PHYTER® Transformerless Ethernet Operation (Rev. A)
Will this topology work for TLK106?
Will this topology work for DP83822H?
Suspect it will work but want to confirm.
Thanks