Part Number: SN65HVD251-Q1
Other Parts Discussed in Thread: SN65HVD255, TCAN1057A-Q1, TCAN1044A-Q1
Hello,
we've been building CAN modules with the SN65HVD251QDRQ1 transceiver chip for years. In our latest board revision, it is having issues communicating reliably in the system. The overall length of shielded twisted pair wire is 80'. We are running at 1Mbps, have two 120 ohm terminations (one at each end), and there are 11 nodes total. We receive error frames with this new build, and never did before. Examining with a scope, we see that the recessive, falling edge is slower in the newest build compared to the original build from 3 years ago. When comparing capacitance of CAN-H and CAN-L in unconnected modules with a calibrated LCR meter, the old device measures less capacitance than the newer modules. The capacitance goes away (to pF) when the transceiver chip is removed. This circuit's schematic hasn't changed. Has the SN65HVD251QDRQ1 chip had any physical changes to it that may have increased the CAN H/L output capacitance or slowed down its edge rates? Our circuit is below.
Bill