Part Number: DS90CF384
Hi Team,
Can I interface 4 bit LVDS signals directly to "DS90CF384" IC receiver?
The display which we shall be using has 24-bit RGB signals and our proccessor has 4-bit LVDS signals terminated. So, we need to convert 4-bit LVDS signals to 24-bit RGB signals. Is the chosen IC suitable for the application, if better options are available I am open for suggestions. If the chosen IC is acceptable, could you please provide a detailed datasheet of the same as the datasheet provided in the website is not detailed.
Thanks and Regards,
Mahima D