Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLIN1431-Q1: PV Ratio Not Correct

Part Number: TLIN1431-Q1

Hi TI,

I am using TLIN14315-Q1, and VCC pin is 5V.

I have 470ohm + 100nF on VBAT pin, and 100ohm+100nF between PV pin and MCU ADC pin.

Then I provide VBAT=12.8V but measure PV pin is 1.42V. The ratio is around 1:9.

I think it should be 1:7 for 5V SBC.

Could you tell me what is going on?