Part Number: DS160PT801
Other Parts Discussed in Thread: LMKDB1202
Hi,
Currently working on a design that integrates the DS160PT801 into a product.
I am looking at the clocking architecture for it. We will be running PCIe Gen4 through this and would like to be able to automatically work in CC or IR mode for clocking.
I had hoped to use the LMKDB1202 device as it appears to have a nice LOS feature where if the REFCLK from the PCIe backplane is not present then it can switch over to using an onboard oscillator.
I was hoping for some confirmation that these two devices are suitable to pair together for this function.
CLKIN0 -> PCIe REFCLK from Connector / Backplane
CLKIN1 -> 100MHz Differential Oscillator
CLKOUT0 -> PCIe Endpoint
CLKOUT1 -> DS160PT801 Input
LOS -> Latch Circuit -> CLK_IN_SEL