Part Number: TCAN4550EVM
Other Parts Discussed in Thread: TCAN4550,
Hello,
we are trting to setup tcan4550 under spi on our embedded linux 6.1
we mange to see the SPI line is sending clock on boot - but can't get the tcan to work
right now we are using the tcan4550evm board - connecting spi to spi
and PIN16 to VBAT to power on the device
this is the device tree we are using :
spi1: spi@fc000000 { //using PA16 for poweron tcan on spi1
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_spi1_default>;
clocks = <&pmc PMC_TYPE_PERIPHERAL 34>;
clock-names = "spi_clk";
status = "okay";
// spidev@0 {
// compatible = "spidev";
// reg = <0>;
// spi-max-frequency = <100000>;
// #address-cells = <1>;
// #size-cells = <1>;
//};
tcan: can@0 {
//Device_Tree: https://docs.zephyrproject.org/latest/build/dts/api/bindings/can/ti,tcan4x5x.html
//Driver: https://git.kernel.org/pub/scm/linux/kernel/git/torvalds/linux.git/tree/drivers/net/can/m_can
//example: https://stackoverflow.com/questions/41828308/reading-writing-spi-devices
compatible = "ti,tcan4x5x";
reg = <0>;
#address-cells = <1>;
#size-cells = <1>;
spi-max-frequency = <1000000>;
// clocks = <&main_xtal>;
clock-frequency = <20000000>;
clocks = <&pmc PMC_TYPE_PERIPHERAL 34>;
clock-names = "spi_clk";
// clock-names = "spi_clk";
// device-state-gpios = <&pioA PIN_PA16 GPIO_ACTIVE_HIGH>;
// device-wake-gpios = <&gpio0 1 GPIO_ACTIVE_HIGH>;
// reset-gpios = <&gpio0 2 GPIO_ACTIVE_HIGH>;
int-gpios = <&pioA PIN_PC5 GPIO_ACTIVE_HIGH>;
// bosch,mram-cfg = <0x0 15 15 5 5 0 10 10>;
bosch,mram-cfg = <0x0 0 0 16 0 0 1 1>;
bus-speed = <250000>;
bus-speed-data = <1000000>;
status = "disabled";
// can-transceiver {
// max-bitrate = <8000000>;
// };
};
};
on demseg we get this:
dmesg | grep spi
atmel_spi fc000000.spi: Using dma0chan0 (tx) and dma0chan1 (rx) for DMA transfers
atmel_spi fc000000.spi: Using FIFO (16 data)
atmel_spi fc000000.spi: registered master spi3
spi spi3.0: setup: bpw 8 mode 0x0 -> csr0 0000000a
spi spi3.0: DEactivate NPCS, mr 000f0031
spi spi3.0: setup mode 0, 8 bits/w, 1000000 Hz max --> 0
atmel_spi fc000000.spi: registered child spi3.0
atmel_spi fc000000.spi: Atmel SPI Controller version 0x311 at 0xfc000000 (irq 153)
tcan4x5x spi3.0: no clock found
tcan4x5x spi3.0: no CAN clock source defined
tcan4x5x spi3.0: setup: bpw 8 mode 0x0 -> csr0 0000000a
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: setup mode 0, 8 bits/w, 1000000 Hz max --> 0
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: activate NPCS, mr 000e0031
atmel_spi fc000000.spi: start fifo xfer (ptrval): len 8 tx (ptrval) rx (ptrval) bitpw 8
tcan4x5x spi3.0: DEactivate NPCS, mr 000f0031
tcan4x5x spi3.0: Unsupported version number: 0
tcan4x5x: probe of spi3.0 failed with error -22
can someone point out what is missing? and what is the problem ?
or where to search for the problem ?
Thank you ,