Part Number: AM26LV31
Hello, may I ask a question about AM26LV31.
My backend servo control differential input requires a VT value between 2.5-3.8V,
1) May I ask if the differential output voltage of this chip can meet the requirements. I have confirmed the datasheet, it seems to be only 1.5V?
2) I tested the output of AM26LV31IDR on my test substrate, and the differential voltage measured using a differential probe was actually 3V Is there any difference between the content on the datasheet and what is it? Is my test inaccurate?
3) This chip is powered by 3.3V, and the same AM26LV31E is also 3.3V. I feel that the VOD of the latter is much larger. Why?
thanks