This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83822I: reading out different register values right after writing

Genius 4270 points

Part Number: DP83822I

Hi,

My customer is using DP83822I and facing the phenomenon below,

・During test that repeating READ and WRITE to the same register via MDIO, The reading values are sometimes different from the last writing values.

Incidence  rate:0.1% ( About 100 times out of 100,000 cycles)

1.  In the customer's case, The 2.2kΩ Pull-up resistor that is required on MDIO line is placed a little far from MDIO pin of DP83822I.

    (the 2,2kΩ is placed on different board, and these 2 boards are connected with 10cm FCC cable)  

Would it be the possible cause of this phenomenon?

2. About the incidence rate, Does this rate could be considered as a normal range?

Thanks,

Go