Part Number: TUSB1104
Hello everyone,
I have developed a prototype of an active cable that uses the redriver TUSB1104 at both ends. I have different cable lengths from the prototype. With the help of an oscilloscope and a USB 3.2 device, I then look at the eye diagram for a data rate of 5 Gbit/s and 10 Gbit/s. I use the compliance patterns of CP0 and CP9. This works pretty well for all lengths and the eye diagrams look very good. At a certain length, however, the CP10 pattern no longer works and one of the re-drivers then fails or no longer reacts to the lfps ping and the power supply drops. What could be the reason for this?
Best regards,
Tobias