This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP401A: No video output on display Riverdi RVT70HSTNWN00

Part Number: TFP401A
Other Parts Discussed in Thread: TFP401

Hello,

I'm currently developing a custom board with a Raspberry PI CM4 interfaced directly via HDMI0.

There is no cable, the diff pairs are routed directely from the CM4  to the TFP401A IC to drive the 7 inch 1024*600 IPS display (Riverdi RVT70HSTNWN00 https://download.riverdi.com/RVT70HSTNWN00/DS_RVT70HSTNWN00_Rev.1.2.pdf)

The issue is that I got no video output at all.

HDMI signals are coming from the Raspberry, TFP401A seems to output data, but the display stays black, the measured output clock is 24.5MHz (input HDMI clock 49MHz).

Config :

Dfo/OCKINV = LOW

PD/ST/PIXS/STAG = HIGH

Here are my schematics:

Best regards, Damien