Hello guys,
I'm using the ISO7221A isolators in my design and was reading some application and design notes on the subject.
I'm a bit confused with SLLA284 - Digital Isolator Design Guide, in figure 21. It seems that ground and power planes are short-cut , and I didn't understand what the author wanted to say in the paraghraph soon after the image.
Another doubt I have is that the text says it's good practice to use small vias in high speed PCB designs. On the other hand, I read in Analog Devices' AN-0971 and AN-1109 that we should use large vias to reduce inductance (these ANs are about isolators as well).
Anyone out there with experience with EMC/EMI certification could demystify these doubts?
Thank in advance,
André.