Part Number: TUSB522P
Other Parts Discussed in Thread: STRIKE
Hello,
In the datasheet, it mentions in section 8.2.2.1 that a resistor is sometimes suggested on the differential pins to pass IEC 61000-4-2 contact +-8kV. I have two questions about this:
1. What does this resistor do? How does it improve the protection for the device if there is already a capacitor to block excess current flow?
2. The recommended ESD protection device, PUSB3FR4, has a clamping voltage of 3V. In section 8.2.2.1 in the datasheet, it says that Resd may be required if the clamp voltage is greater than 4V. In table 8-2, despite PUSB3FR4 having just 3V clamping voltage, it recommends a 2.2ohm resistor to pass IEC61000-4-2. Why is this resistor recommended here?
Thank you!
Best regards,
Zach Kimble