Part Number: DS90UB9722-Q1
Dear Team,
in DS is stated if ADC on DS90UB9722-Q1 measure voltages up to 1.207V.
Our questions is:
-> if VDDIO is connected to 1.8V then ADC input ( GPIO0 or GPIO1) is tolerant up to 1.8V but it will measure the same value for 1.207V and 1.8V is that correct?
-> if VDDIO is connected to 3.3V then ADC input ( GPIO0 or GPIO1) is tolerant up to 3.3V but it will measure the same value for 1.207V and 3.3V is that correct?
Best Regards,
d.