Other Parts Discussed in Thread: TUSB9261, TUSB9260
My new design includes a TI TUSB9261 (USB3.0 to SATA bridge). Connected to the TI part is a SPI Flash. On page 10 of the online TI implementation guide for the TUSB9261 states they have tested the Atmel AT25FS010 and Numonyx M25P10A SPI flash chips as being compatible with the TI part.
The Atmel part is now listed as “not recommended for new designs”. The Numonyx is listed as “declining” , being an older part. I had designed in the Atmel part. So here are my questions:
1) Are there newer SPI flash chips that TI recommends as being compatible with the TUSB9261 part now (i.e. someone has tested them)?
2) Are there any SPI flash chips that are known to be incompatible with the TI part, (or programming firmware)?
3) Would an Atmel AT45DB011D http://www.atmel.com/dyn/resources/prod_documents/doc3639.pdf be compatible with the TI part? This is Atmel’s suggested replacement. The only issue with this Atmel replacement is that it is not pin compatible with the original suggesting SPI flash chips.
4) Will the TI programming firmware support writing to an AT45DB011D?
5) Any other thoughts on this subject?
Thanks, and Best Regards,
-Tim Starr on behalf of MS@BA