Part Number: TIC10024-Q1
Other Parts Discussed in Thread: TIC12400-Q1
Hello,
I am planning to use the TIC10024-Q1 in a 12 V automotive ECU.
I want to connect 10 switch to 12 V battery to pins IN0-IN9 of the TIC10024-Q1.
Does the TIC10024-Q1 support test pulses from ISO 7637-2 on its input pins IN0-IN9 without additional external circuits (TVS, diode, resistive divider)?
I have seen the application note "Protecting 12-V MSDI Devices in a 24-V System", but it is dedicated to 24 V systems.
I assume that a TVS and a diode are mandatory to protect the TIC10024-Q1 from voltage transients even in 12 V systems, but this solution limits the flexibility of the MSDI.
Thank you in advance,
Luca