Part Number: TLIN1431-Q1
Hello,
I am using the TLIN1431 part in our project and noticed a strange behavior: if the watchdog is not serviced after the initial configuration the SBC will also cut the VCC after 16 watchdog resets
The only register that seem to affect this behavior is FSM_CONFIG Register (Address = 17h). in the Initial config I set it to 1.
If I leave the default value the VCC pulldown does not happed.
Can you explain this
?
Thank you!
Razvan