Part Number: DP83822HF
Hi Team,
While Referring to DP83822 Trouble Shooting Guide , Under Section 2..4.2 Probe the RBIAS pin, it says following
Measure the DC value of the voltage across the RBIAS resistor and confirm that the voltage is 2.7 V
But while measuring the same, We are getting 0.925V. Can you please update why its happening?
Another Query:
0x0421 Analog Power Detect Status (DP83822 DataSheet) -
When I read it from Registers (phytool read eth0/2/0x0421) , I am getting Value 0x7849 which translates to following
AVD Detected as 1.8V (as per Register Value)
VDDIO detected as 2.5V
But When I probe them, I am getting 3.3V on both AVD & VDDIO
Can you explain why this is happening?