This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THVD1451: VOCM Voltage

Part Number: THVD1451
Other Parts Discussed in Thread: SN74LVC2G86, DS26LS32MQML, DS26LS31C, AM26LV31E, AM26C32, AM26LV32E, AM26C31, AM26C31-EP, AM26C31M, DS26C31MQML, SN75179B

Dear Team, 

Our requirements is to convert single ended TTL input to Differential TTL Output with Common Mode Voltage -1.65V. As per Datasheet VOCM is VCC/ 2  to 3V.  When we use VCC= 3.3VDC then we will get VOCM = 1.65V. 

As per datasheet Is it possible to get VOCM = 3.3V. How can we change VOCM and fixed it to 1.65V. 

Please guide.