Part Number: DS125DF111

If I change the value of register 0x07 : 0x03'h in the control/shared register set, I think it will work as loopback. Is that right?
0xff 0x00 Select control/shared Register
0x07 0x03 input A --> Output B and input B --> output A
I want to set it up as above.
Even if both port A and port B are looped back and the bypass mode is executed, it does not loop back.
Can the DS125DF111 operate as shown in the picture above?
What settings should I set if I can?