Part Number: TCA9517A
Other Parts Discussed in Thread: TCA9800
TCA9517Aについて教えていただけますか?TCA9517Aについて教えていただけますか?回路図を添付します。
I2Cの不具合でMPUの動作が止まる。kairo.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi User4961418,
The reason for the two different VOL levels on A-side and B-side is inherent to the device design. Please see the VOL levels as listed in the datasheet.

When driving from A-side to B-side a logic low signal, we can expect VOLB = 0.52V typical.
Regards,
Tyler
User4961418,
I believe you asked the question:
"The I2C specification of the engineering machinery provides the required data in the medium term. How can we predict the way in which we work?"
I am not sure that I understand your question. Can you restate your question?
Regards,
Tyler
Mr. Taylor, is this voltage suitable for the I2C standard? Is there a way to lower the voltage a little more? Regards,Taro
Taro,
The static voltage offset is not configurable to make lower. It is a set voltage between 0.45V and 0.6V.
As for the i2c standard, VIL = 30% of VCC. Technically the lowest voltage that can be used on the B-side is VCC = 3.3V. 1.8V logic cannot work on B-side due to static voltage offset. Also, minimum VCCB = 2.7V.
If 1.8V logic is need on B-side, try looking at lower voltage options such as the TCA9800 / TCA980x series of devices.
Regards,
Tyler