Part Number: TPD2S017
Hi Team
This is my first question. Please help me.
I use the chip TPD2S017 for protection USB.
When initializing the USB on the MCU, even without plugging in the USB, the data signal changes to high, and 3.5 volts is measured on VUSB.
The issue is that I'm currently measuring 3.5 volts.
The reason is that I am also using the VUSB line for other purposes.
So, how can I make VUSB go low when the USB is not connected?
Thanks.