This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HD3SS3412: HD3SS3412 Power Dissipation Changes

Part Number: HD3SS3412

Hi TI Team,

I would like to ask what is the changes on the part why the power dissipation become  MIN = 2.8mW, MAX = 4.4mW? Original rating is MIN = 15.5mW, MAX = 21.6mW.

We used this IC in our board and we created a checker to check the current of the device. Initially, we set the limits to 2mA and 6mA. We fabricated new board, unfortunately, failed on lower limits since the measure current is only 1mA. We replaced the IC several times and still reading is 1mA. Swap the passing and failing IC and failure transferred. Upon checking the datasheet, power dissipation is changed that's why current become 1mA only. I hope you will notice my inquiry.

Thanks,

Cian