Part Number: DP83869HM
Hi,
We have used parts in our ethernet design
1) TI's PHY DP83869HM
2) Magnetics from pulse electronics (10/100Base-T)
3) M12 connector from Amphenol (MFR# M12D-04PFFC-SF8B15)
Now, after magnetics MDI signals are coming to board edge and M12 connector with termination type wire leads is connected on back-panel of product.
If I connect wire leads of M12 connector with MDI signals through normal header (pitch: 1.27mm), there will be an impedance mismatch at this point. So, are there any recommended connectors or any other way using which ethernet trace impedance will be affected minimally?
P.S. I cannot use PCB mounted M12 connectors due to space limitation.
Thank you and regards,
Nikhil Jadhav