Part Number: TUSB320
Other Parts Discussed in Thread: TPS61023,
Hello sir,
I have been using a TUSB320 in DRP mode for my application and using TPS61023 as a boost converter. My battery charging circuitry is working very well. But when I try to charge an external device such as mobile phone. Some of the phones shows charging status but they give an option of slow charging. while the other phone do not even give the charging status. It is to be noted that I have configured the CC pins to 1.5A for now. But when I change them to 3A then none of the device shows the charging status. Kindly assist me in this regard. I am attaching my schematic and PCB layout. Thanks