Part Number: PCA9555
Other Parts Discussed in Thread: TCA9555
Hi team,
My customer has a abnormal issue for PCA9555. They found that after power on, the input register 0 and 1 are all inverted. And after they write 0 to register 4 and 5. The input register 0 and 1 become normal. Do you have any insight for it? I attached the SCH and the start up waveform: red is the 3.3V power; Yellow is SDA and Blue is SCL. also, the waveform looks strange too. The schematic shows it's NXP's part, but confirmed that they are using TI's part for this test, and NXP's part do not have this issue.
THanks
Han

riser2-1_x16 x16 PCIe RiserBF_SCH_SDV_PASS2_20240129-BOMCHANGE.pdf