Part Number: DP83867CR
Hi,
I have updated the DP83867 Linux driver to support cable testing, but I am encountering a problem when testing a cable that is connected correctly.
When testing cables with known Open and Short Circuits, the results are accurate. However, when I test a cable that is connected correctly at both ends, the expected result should be "OK," but I am receiving an "Open Circuit" error instead.
I printed the register values and observed that the peak values are never lower than the threshold in the last measurement. This discrepancy causes the fault type to be reported as an Open Circuit.
Below, I have added an image of a test result where Pair A reports "OK," but Pair B reports "Open Circuit" despite the cable being connected correctly.

Does any one know what can cause the high peak_value when the cable is connected correctly?
Kind regards,
Mart