Part Number: DP83TC811-Q1
Other Parts Discussed in Thread: DP83TC811
I configured the DP83TC811 to Test Mode 1 according to document snla276, but the output speed should be 10BASE-T1. Can you provide the REG settings for 100BASE-T1?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83TC811-Q1
Other Parts Discussed in Thread: DP83TC811
I configured the DP83TC811 to Test Mode 1 according to document snla276, but the output speed should be 10BASE-T1. Can you provide the REG settings for 100BASE-T1?
Hello Kung,
Our DP83TC811 PHY is only a 100BASE-T1 PHY, it is a single speed PHY with no 10BASE-T1 capability.
Regards,
Avtar
Hello Kung,
I have run test mode 1 on our EVM board, and saw a period of 1.740 us. When looking at our PMA compliance report for Test mode 1 the period is roughly 1.740 us and that test passed compliance. Are you seeing issues passing compliance or are you asking about the period of the waveform?
Regards,
Avtar
Hello Kung,
I see that you have passed for test mode 1, are you maybe referring to the comments where it says signal validation?
Regards,
Avtar
Yes, I compared the standard signal of Tektronix and found the problem shown in the picture above
Hello Kung,
I am having trouble finding where Tektronix standard shows 100BASE-T1 period has to be 1.2 ns, I see 100BASE T1 standard says droop has to be atleast 500ns.
Also where is 10BASE-T1 standard saying 1.740 us?
Regards,
Avtar
According to the specifications of 100BASE-T1 (IEEE802.3bw) and the test standards, the definition of Test Mode 1 is as follows in the specification screenshot: Therefore, the period of Test Mode 1 => 34+1/34-1 symbols ~ 40+1/40-1 symbols, and the symbol rate of 100BASE-T1 is 66.66 MHz = 15 ns. The correct period for Test Mode 1 is (34*2)15 ns = 1.02 µs ~ (402)*15 ns = 1.2 µs, which falls within the Tektronix software's check range.





Hello Kung,
Thank you for sharing the screenshots, I see however that the minimum value of N shall be 34 symbols in order to achieve a symbol period greater than 500 ns. This is the only hard requirement seen in this document and that is why with a period of 1.740 ns our PHY passes this Test mode 1 compliance.
Regards,
Avtar
Hello Kung,
I am glad. Let us know if you have any further questions.
Regards,
Avtar