Part Number: SN65HVD10
Other Parts Discussed in Thread: THVD2410
Hi
we have RS485 support VCC=3.3V with internal charge pump so Voh can be 4.7V as VCC=5V spec?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gareth,
Are you looking for a device suggestion that can take 3.3V but the TTL output provides a VoH around 5V?
I believe the only device family we have that has adjustable level shifting is the THVD24xx family (like THVD2410) but the recommended operating max for Vio is up to Vcc.
You probably need to look into using a level shifter after the TTL signal.
-Bobby