Part Number: DP83826I
Dears:
customer found some question between datasheet and EVM, Please refer to attachment. Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DP83826I
Dears:
customer found some question between datasheet and EVM, Please refer to attachment. Thanks.
Hi Haiwen,
Please allow me until Thursday 5/23 to review these questions and get back to you with feedback.
Thank you,
Evan
Hi Haiwen,
Please see my feedback below:
1) Please refer to 8.5 Electrical Characteristics for voltage levels of the Analog pins. These pins (TD, RD, XI, XO, ...) do not follow VDDA level.
2,3) For CEXT and transformer termination capacitor, please use datasheet capacitor value 2nF. EVM capacitor value is outdated, sorry for the confusion here.
4) RMII slave/master configuration bits are in register 0x468.
Thank you,
Evan
Hi Evan:
In DP83826I datasheet , "9.4.1 Hardware Bootstraps Configuration" describes "Configuration of the device may be done through the strap pins or through the management register interface."; but I cannot find the registers that control RMII Slave/Master. Could you please help give a guide ? Thanks .
Hi Haiwen,
Please refer to register 0x17[7]:

25MHz clock reference = RMII Master mode
50MHz clock reference = RMII Slave mode
This assumes RMII is enabled with 0x17[5] = '1' or through straps.
Thank you,
Evan